Skip to main content

Tour the Logic

Every feature of the new Logic BSC has been re-examined, re-engineered and reimagined, introducing many innovative features. At the core is Logic OS, accessed through an innovative 5” touchscreen interface within the cabinet interior.

Articles

Labconco's New Logic® Biosafety Cabinet Revolutionizes Laboratory Safety and Performance – Again

Announcing the launch of Labconco’s redesigned Logic Biosafety Cabinet (BSC).

Read More ➔

Unique features of Logic Class II Biosafety Cabinets

Labconco’s all-new fourth-generation Logic Class II Biosafety Cabinets are packed full of innovative features that enhance how you do science safely.

Read More ➔

What are the biosafety cabinet classes?

Biological safety cabinet classes (or biosafety cabinet classes) are categories describing how the cabinet works and what it protects. These “categories” are Class I, Class II and Class III.

Read More ➔

Laminar flow in the laboratory: What you need to know

While laminar flow helps to reduce turbulence, turbulent flow encourages it by creating unintentional swirls of air that place particles randomly on surfaces within an enclosure...

Read More ➔

Mitigating Microbial Risk: Biosafety Cabinet eBook

Our ebook will guide you to the answers you need. Start with general guidance, then take a deeper dive into selecting the right biological safety cabinet for your application, laboratory safety tips and other useful subjects for microbiologists and other biological safety cabinet users.

Get my eBook