Contact
Adam Keithley | Vice President, Channel Management, Labconco
P R E S S R E L E A S E
For release: April 15, 2025
KANSAS CITY, Missouri – Labconco® Expands CentriVap™ Line with New Pro Models, Enhanced Features
Labconco Corporation unveils the redesigned CentriVap™ Pro Centrifugal Concentrator, a breakthrough in speed, precision and efficiency for sample concentration. With this launch, Labconco expands the CentriVap portfolio to include both the advanced Pro models and standard models, offering laboratories flexibility in selecting the best fit for their applications. Engineered to tackle the growing demands of modern laboratories, the new Pro models combine next generation technology with an intuitive user experience, streamlining workflows and giving researchers unprecedented control over sample integrity.
“Today’s scientists and researchers need more than just a concentrator; they need an efficient system that adapts to their unique research needs,” says Labconco’s Product Manager Zachary Zakibe. “With the CentriVap Pro and CentriVap Standard Concentrators, we’ve created a range of solutions that enhance sample integrity, speed up processing and give researchers the flexibility they need.”
The CentriVap Pro is a fully connected solution that puts powerful new controls at scientists’ fingertips. With VaporWorks™ OS, laboratories can optimize every step of the concentration process with customizable run parameters and method storage. The new 5" touchscreen display provides effortless control over run settings, real-time data monitoring and diagnostics. Researchers can now easily program vacuum pressure, rotor speed and temperature to optimize their workflow. Additionally, the CentriVap Pro introduces a beneficial End Point Assist system, for use with total sample volumes over 36 ml and temperatures above 40° C
Labconco’s Director of Laboratory Products Kelly Williams says, “We understand the importance of controlling parameters and conditions to which samples are exposed. The CentriVap Pro isn’t just faster – it’s smarter, giving scientists greater control and confidence in their results.”
For researchers needing high throughput, the stackable rotor design doubles sample capacity without taking up additional bench space. Researchers can now process up to 312 samples at once, streamlining workflows and reducing turnaround times.
Every lab has unique sample challenges, and the CentriVap Pro is built to meet them. Multiple specialized configurations are tailored for temperature-sensitive samples, aggressive solvents, and high-throughput DNA processing.
The Refrigerated CentriVap Pro offers cooling to -10° C and heating to +100° C, making it ideal for protecting heat-sensitive samples like RNA and proteins.
The Acid-Resistant CentriVap Pro is built to handle harsh chemicals with a PTFE-coated chamber, Hastelloy drive shaft and chemical-resistant components.
For nucleic acid research, the DNA CentriVap Pro comes fully equipped with a built-in diaphragm vacuum pump, dual vapor traps and a stainless-steel DNA rotor that’s ready to use right out of the box
“Every CentriVap Pro model is designed for efficiency, durability and precision to ensure your lab gets the most out of every run – every time,” Zakibe adds.
To celebrate this launch, Labconco is including a free CentriZap™, an exclusive Labconco accessory that allows you to visually inspect samples as if they were standing still, even while they’re moving at 1800 RPM. It will be free with every CentriVap Pro model purchased by December 31, 2025.
Labconco has spent the past century designing laboratory equipment that empowers scientists and researchers to focus on discovery, not troubleshooting. The addition of the CentriVap Pro to the CentriVap line embodies this commitment. Labconco provides a concentrator for all labs, whether they need high capacity with smarter controls, or a simple, efficient solution.
For more information or to explore configurations tailored to your research needs, visit labconco.com/centrivap.
About Labconco
Labconco Corporation celebrates 100 years of driving science forward. Since 1925, we’ve partnered with scientists to create equipment that protects people, preserves discoveries, and expands the boundaries of innovation. Trusted worldwide, our biosafety cabinets, fume hoods, freeze dryers and other equipment solutions have supported breakthroughs in medicine, forensics and environmental science. As we honor our century of excellence, we’re driven to shape the next century of discovery.