Fayetteville, AR | Educational Institution
Discovery Hall is a multi-level, multidisciplinary space dedicated to chemistry teaching labs, bio-anthropology and archaeology.
Wellesley, MA | Educational Institution
Two challenges were overcome with one solution when constructing the new Science Center on Science Hill at Wellesley. The mechanical system needed to support the number of fume hoods required seemed impossible, and providing temporary chemical labs during construction created unique challenges as well. Labconco had one elegant and complete answer for both problems.
Northfield, MN | Educational Institution • Zero Net Energy Labs • Sustainable Lab Design
This Zero Net Energy laboratory project had particular needs that focused on not only the sustainability of the technology chosen, but also its flexibility.
West Lafayette, IN | Educational Institution
Labconco added airfoils on the sides of the hoods where custom rising marker boards were installed, and compensated for the extra weight by reinforcing the equipment for optimum safety, performance and longevity.
Wichita, KS | Forensic Laboratories • Educational Institution
Besides adequate space and advanced scientific equipment, KBI had another unique need: a safe and effective way to teach these methods to others—specifically, to the students in the forensic sciences department at Washburn University.
Madison, WI | Industrial, Manufacturing or Utility
Labconco’s team worked hand in hand with Eurofins and their lab architects to develop a trusting and meaningful relationship, through countless hours of design and strategy, dozens of custom drawings, and hundreds of messages. The result is this amazing laboratory space that boasts a total of 72 purpose-built fume hoods.
Pittsburgh, PA | Biopharma
This lab space has since expanded and a new wing of the lab was created to accommodate the additional R&D research.
Kansas City, MO | Sustainable Lab Design
Kansas City, MO | Pharmacy Institutions
Louisville, CO | Industrial, Manufacturing or Utility • Biopharma
One of our high-profile pharma research clients recently expanded and had a need for custom fume hoods with the goal of rapidly delivering new medicines for people with cancer.
Mexico City, DF | Educational Institution • Sustainable Lab Design
This university is recognized as one of the top private higher education institutions offering undergraduate, graduate and technical degrees in Mexico and Latin America.
Kansas City, MO | Industrial, Manufacturing or Utility • Sustainable Lab Design
The Athena Mobile Lab was designed to function as a highly customizable laboratory. It can be outfitted with a wide selection of state-of-the-art sample preparation, containment and analytical solutions for chemical, biological or mechanical testing.
Pittsburgh, PA | Educational Institution
Braskem America stands as the premier producer of thermoplastic resins in the Americas and the largest producer of polypropylene in the U.S.