Skip to main content
GettyImages-1267748023

Best Practices for Handling Potentially Hazardous Mail

On February 2, 2025
Posted in Articles

Safety of operators processing potentially hazardous mail is an often overlooked process in high-risk environments where dangerous substances might be encountered. For over 20 years, concerns surrounding hazardous materials in mail have escalated, beginning with the anthrax attacks in the early 2000s and continuing with today’s heightened risks involving synthetic opioids like fentanyl. Given the highly potent nature of these substances, it is imperative for individuals working in mailrooms and receiving departments to utilize advanced containment methods to maximize personal safety.

At-risk facilities must implement comprehensive safety measures to mitigate the potential dangers associated with contaminated mail. This article outlines key methods for maintaining safe mail-handling practices, focusing on proper containment, personal protective equipment (PPE), and process improvements to reduce exposure risks.

Understanding the Threats

The risks posed by contaminated mail include exposure to chemical, biological, and radiological hazards. Highly toxic substances like anthrax spores, ricin, and synthetic opioids such as fentanyl are particularly dangerous because fatal amounts can easily be transmitted in common packages. Fentanyl, for example, is 50 to 100 times more potent than morphine, making even trace amounts deadly to those who come into contact with it. Exposure through inhalation, skin contact, or accidental ingestion can result in severe health complications or even death.

Key Safety Strategies for Handling Suspicious Mail

To ensure safety when dealing with potentially hazardous mail, it's crucial to adopt a multi-layered approach that includes physical containment, protective gear, and improved operational protocols. Below are three essential steps every facility should follow.

1. Proper Containment of Suspicious Mail

Containment is the first line of defense against hazardous materials in the mail. To prevent airborne contaminants from escaping and posing a risk to staff, all mail handling should occur in specialized containment equipment designed for the capture of harmful particles

  • Use a HEPA Filtered Containment Hood: A HEPA filtered containment hood specifically engineered for hazardous substances is essential for user safety. These hoods feature HEPA filtration systems that effectively capture hazardous particulates like drug powders or biohazards. Standard fume hoods are inadequate for containment purpose because they lack sufficient filtration in the exhaust pathway, thus allowing dangerous powders to contaminate the ductwork and rooftop where the exhaust exists the building.

  • Consider Hood Size & Customization: The containment hood must be large enough to accommodate not just packages, but also any tools, such as letter opener instruments or automated mail processors. Customized solutions may aid when instruments, extra large bins, or other equipment do not fit in standard hoods. A custom-sized hood might be necessary if standard dimensions do not meet your operational needs.

  • Annual Certification and Maintenance: The hood must be certified annually by a qualified technician to ensure its optimal performance. Certification should include a thorough leak test on the HEPA filter, calibration of airflow speeds, and an evaluation of the hood’s containment abilities in its current setup. A well-maintained hood is critical to preventing leaks of dangerous substances.

  • Placement Considerations: Position the hood in a low-traffic, stable environment, away from areas with high airflow disturbances such as doors, hallways, or return air ducts. This helps ensure consistent airflow and improves containment effectiveness.

2. Personal Protective Equipment (PPE) Wearing appropriate PPE is non-negotiable when processing potentially dangerous mail. PPE forms the second layer of defense and offers protection in case containment measures fail or hazards are inadvertently released.

  • Basic PPE: Workers should always wear gloves, protective eyewear, and a lab coat or coveralls when handling suspicious mail. This protects against direct contact with harmful substances that could be present on the exterior of packages or released during processing.

  • Respiratory Protection: If there is any risk of aerosolization—where hazardous particles become airborne—staff should wear a suitable mask or respirator. Respirators are particularly important when dealing with potent synthetic opioids like fentanyl, which can be harmful even in near-invisible quantities.

3. Improve Protocols to Minimize Exposure Beyond containment and PPE, refining operational protocols is essential to maintaining a safe work environment. Regularly updating and following best practices can significantly reduce the risk of exposure.

  • Pre-Processing Containment: Always place suspicious mail into the powder containment hood before beginning any handling activities. Ensure proper procedures are followed to maintain safety throughout processing.

  • Avoid Overcrowding: Overloading the hood with too many items can disrupt airflow and reduce containment efficiency. If necessary, use additional containment spaces for unprocessed mail to ensure proper air circulation in the working hood.

  • Open Mail Slowly: Minimize disruption by opening mail carefully and deliberately. Use a box cutter or letter opener to easily open a package, instead of ripping items – which creates aerosols. Keep your hands at least 4 to 6 inches inside the hood to ensure maximum containment. Sudden or rapid movements may stir up hazardous particles and compromise safety.

  • Proper Equipment Usage: If using automatic mail openers, confirm that the containment hood is large enough to fully house the device. Position the opener toward the back of the enclosure to reduce the risk of contaminant escape during use.

  • Waste and Spill Management: Plan for potential waste and spills by organizing the workspace within the hood. Built-in waste chutes, shelves, and proper disposal containers should always be used to keep materials and tools within easy reach while maintaining cleanliness and order.

Conclusion Handling hazardous mail requires meticulous attention to detail and adherence to established safety protocols. Proper containment systems, the right personal protective equipment, and continuous improvements to handling procedures will significantly reduce risks. For facilities where exposure to hazardous materials is a concern, proactive safety measures are essential to protect workers from harm. Ensuring that containment hoods are properly maintained, that appropriate PPE is always used, and that operational protocols are followed will minimize the risks posed by dangerous substances in the mail.

Further Reading:

Learn more about the risks of fentanyl exposure

NIOSH

Explore available containment solutions for mail safety

Filtered Glove Boxes